Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MathIntegrationBuilder.AssociativityTypes |
MathIntegrationBuilder.AssociativityTypes.EXISTING
Maintain associativity to the worksheet
|
static MathIntegrationBuilder.AssociativityTypes |
MathIntegrationBuilder.AssociativityTypes.NEW
Make associative to the worksheet
|
static MathIntegrationBuilder.AssociativityTypes |
MathIntegrationBuilder.AssociativityTypes.NONE
No associativity to the worksheet
|
Modifier and Type | Method and Description |
---|---|
MathIntegrationBuilder.AssociativityTypes |
MathIntegrationBuilder.associativityType()
Returns the option to control associativity to the equation
License requirements: None. |
static MathIntegrationBuilder.AssociativityTypes |
MathIntegrationBuilder.AssociativityTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MathIntegrationBuilder.AssociativityTypes |
MathIntegrationBuilder.AssociativityTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MathIntegrationBuilder.AssociativityTypes[] |
MathIntegrationBuilder.AssociativityTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MathIntegrationBuilder.setAssociativityType(MathIntegrationBuilder.AssociativityTypes associativityType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.