Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.AXIS
axis
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.BODY_COLLECTOR
body collector
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.CSYS
csys
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.CURVE
single curve or edge
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.CURVE_COLLECTOR
curve collector or edge collector
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.FACE
single face or datum plane
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.FACE_COLLECTOR
face collector
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.OBJECT
general geometry such as the target body and the tool body for copying unite feature
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.PLANE
plane
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.POINT
point
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.SECTION
section
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.UNDEFINED
default type for feature name lable
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.VECTOR
vector
|
Modifier and Type | Method and Description |
---|---|
MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.type()
Returns the matchedReference type
License requirements: None. |
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MatchedReferenceBuilder.Types |
MatchedReferenceBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MatchedReferenceBuilder.Types[] |
MatchedReferenceBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MatchedReferenceBuilder.setType(MatchedReferenceBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.