Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static LinearDimensionBuilder.OrientationOptionType |
LinearDimensionBuilder.OrientationOptionType.ORIENT_XPRESS
Orientation option using Orient Xpress
|
static LinearDimensionBuilder.OrientationOptionType |
LinearDimensionBuilder.OrientationOptionType.VECTOR
Orientation option using vector
|
Modifier and Type | Method and Description |
---|---|
LinearDimensionBuilder.OrientationOptionType |
LinearDimensionBuilder.orientationOption()
Returns the option that controls whether the OrientXpress or whether the vector block
Controls the orientation of the Linear Dimension
License requirements: None. |
static LinearDimensionBuilder.OrientationOptionType |
LinearDimensionBuilder.OrientationOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LinearDimensionBuilder.OrientationOptionType |
LinearDimensionBuilder.OrientationOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LinearDimensionBuilder.OrientationOptionType[] |
LinearDimensionBuilder.OrientationOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LinearDimensionBuilder.setOrientationOption(LinearDimensionBuilder.OrientationOptionType orientationOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.