Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static LawExtensionBuilderEx.MiterOptions |
LawExtensionBuilderEx.MiterOptions.BLEND
Creates a three-sided patch between two faces
|
static LawExtensionBuilderEx.MiterOptions |
LawExtensionBuilderEx.MiterOptions.NONE
No miter solution between two discontinuous faces
|
static LawExtensionBuilderEx.MiterOptions |
LawExtensionBuilderEx.MiterOptions.RADIUS
Creates a four-sided patch between two faces
|
static LawExtensionBuilderEx.MiterOptions |
LawExtensionBuilderEx.MiterOptions.SHARP
Creates a sharp edge between two faces
|
Modifier and Type | Method and Description |
---|---|
LawExtensionBuilderEx.MiterOptions |
LawExtensionBuilderEx.miterOption()
Returns the miter option
License requirements: None. |
static LawExtensionBuilderEx.MiterOptions |
LawExtensionBuilderEx.MiterOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LawExtensionBuilderEx.MiterOptions |
LawExtensionBuilderEx.MiterOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LawExtensionBuilderEx.MiterOptions[] |
LawExtensionBuilderEx.MiterOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LawExtensionBuilderEx.setMiterOption(LawExtensionBuilderEx.MiterOptions miterOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR free_form_modeling ("FREE-FORM MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.