Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static LawExtensionBuilder.OppositeSideExtensionOptions |
LawExtensionBuilder.OppositeSideExtensionOptions.ASYMMETRIC
Asymmetric extension
|
static LawExtensionBuilder.OppositeSideExtensionOptions |
LawExtensionBuilder.OppositeSideExtensionOptions.NONE
No extension on opposite side
|
static LawExtensionBuilder.OppositeSideExtensionOptions |
LawExtensionBuilder.OppositeSideExtensionOptions.SYMMETRIC
Symmetric extension
|
Modifier and Type | Method and Description |
---|---|
LawExtensionBuilder.OppositeSideExtensionOptions |
LawExtensionBuilder.oppositeSideExtensionOption()
Returns the opposite side extension option
License requirements: solid_modeling ("SOLIDS MODELING") OR free_form_modeling ("FREE-FORM MODELING") . |
static LawExtensionBuilder.OppositeSideExtensionOptions |
LawExtensionBuilder.OppositeSideExtensionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LawExtensionBuilder.OppositeSideExtensionOptions |
LawExtensionBuilder.OppositeSideExtensionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LawExtensionBuilder.OppositeSideExtensionOptions[] |
LawExtensionBuilder.OppositeSideExtensionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LawExtensionBuilder.setOppositeSideExtensionOption(LawExtensionBuilder.OppositeSideExtensionOptions oppositeSideExtension)
License requirements: solid_modeling ("SOLIDS MODELING") OR free_form_modeling ("FREE-FORM MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.