Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static LatticeBuilder.LatticeTypes |
LatticeBuilder.LatticeTypes.CONFORMAL_GRAPH |
static LatticeBuilder.LatticeTypes |
LatticeBuilder.LatticeTypes.SURFACE_GRAPH |
static LatticeBuilder.LatticeTypes |
LatticeBuilder.LatticeTypes.TETRAHEDRON_GRAPH |
static LatticeBuilder.LatticeTypes |
LatticeBuilder.LatticeTypes.UNIT_GRAPH |
Modifier and Type | Method and Description |
---|---|
LatticeBuilder.LatticeTypes |
LatticeBuilder.latticeType()
Returns the type of lattice that is going to be created.
|
static LatticeBuilder.LatticeTypes |
LatticeBuilder.LatticeTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LatticeBuilder.LatticeTypes |
LatticeBuilder.LatticeTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LatticeBuilder.LatticeTypes[] |
LatticeBuilder.LatticeTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LatticeBuilder.setLatticeType(LatticeBuilder.LatticeTypes latticeType)
License requirements: nx_lattice_base (" NX Lattice Base") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.