Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static IsoclineCurveBuilder.CurveTypes |
IsoclineCurveBuilder.CurveTypes.MULTIPLE |
static IsoclineCurveBuilder.CurveTypes |
IsoclineCurveBuilder.CurveTypes.SINGLE |
Modifier and Type | Method and Description |
---|---|
IsoclineCurveBuilder.CurveTypes |
IsoclineCurveBuilder.isoclineTypes()
Returns the isocline types
License requirements: None. |
static IsoclineCurveBuilder.CurveTypes |
IsoclineCurveBuilder.CurveTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IsoclineCurveBuilder.CurveTypes |
IsoclineCurveBuilder.CurveTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IsoclineCurveBuilder.CurveTypes[] |
IsoclineCurveBuilder.CurveTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IsoclineCurveBuilder.setIsoclineTypes(IsoclineCurveBuilder.CurveTypes isoclineTypes)
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.