Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static IFormBuilder.ParameterDirectionOptions |
IFormBuilder.ParameterDirectionOptions.ISO_U
Iso-U direction
|
static IFormBuilder.ParameterDirectionOptions |
IFormBuilder.ParameterDirectionOptions.ISO_V
Iso-V direction
|
Modifier and Type | Method and Description |
---|---|
IFormBuilder.ParameterDirectionOptions |
IFormBuilder.parameterDirection()
Returns the iso-parameter direction
License requirements: None. |
static IFormBuilder.ParameterDirectionOptions |
IFormBuilder.ParameterDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IFormBuilder.ParameterDirectionOptions |
IFormBuilder.ParameterDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IFormBuilder.ParameterDirectionOptions[] |
IFormBuilder.ParameterDirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IFormBuilder.setParameterDirection(IFormBuilder.ParameterDirectionOptions parameterDirection)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.