Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static IFormBuilder.InsertionMethodOptions |
IFormBuilder.InsertionMethodOptions.BETWEEN_POINTS
Insert curves between points
|
static IFormBuilder.InsertionMethodOptions |
IFormBuilder.InsertionMethodOptions.THROUGH_POINTS
Insert curves through points
|
static IFormBuilder.InsertionMethodOptions |
IFormBuilder.InsertionMethodOptions.UNIFORM
Insert curves uniformly
|
Modifier and Type | Method and Description |
---|---|
IFormBuilder.InsertionMethodOptions |
IFormBuilder.insertionMethod()
Returns the iso-parameter curve insertion method
License requirements: None. |
static IFormBuilder.InsertionMethodOptions |
IFormBuilder.InsertionMethodOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IFormBuilder.InsertionMethodOptions |
IFormBuilder.InsertionMethodOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IFormBuilder.InsertionMethodOptions[] |
IFormBuilder.InsertionMethodOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IFormBuilder.setInsertionMethod(IFormBuilder.InsertionMethodOptions insertionMethod)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.