Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Interface and Description |
---|---|
interface |
InstanceFeature
Represents a instance feature
To create or edit an instance of this class, use InstanceFeatureBuilder Created in NX8.0.0 |
interface |
Mirror
Represents a mirror feature.
|
interface |
PatternFeature
Represents a pattern feature
To create or edit an instance of this class, use PatternFeatureBuilder Created in NX7.0.0 |
interface |
PatternGeometry
Represents a pattern geometry feature.
|
Modifier and Type | Method and Description |
---|---|
IContainerFeature |
Feature.containerFeature()
Returns the container feature for this feature.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.