Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HoleFeatureBuilder.HoleSubtype |
HoleFeatureBuilder.HoleSubtype.COUNTERBORE
Counterbore hole
|
static HoleFeatureBuilder.HoleSubtype |
HoleFeatureBuilder.HoleSubtype.COUNTERSINK
Countersink hole
|
static HoleFeatureBuilder.HoleSubtype |
HoleFeatureBuilder.HoleSubtype.SIMPLE
Simple hole
|
Modifier and Type | Method and Description |
---|---|
HoleFeatureBuilder.HoleSubtype |
HoleFeatureBuilder.subtype()
Returns
the type of hole
License requirements: features_modeling ("FEATURES MODELING"), solid_modeling ("SOLIDS MODELING") . |
static HoleFeatureBuilder.HoleSubtype |
HoleFeatureBuilder.HoleSubtype.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HoleFeatureBuilder.HoleSubtype |
HoleFeatureBuilder.HoleSubtype.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HoleFeatureBuilder.HoleSubtype[] |
HoleFeatureBuilder.HoleSubtype.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HoleFeatureBuilder.setSubtype(HoleFeatureBuilder.HoleSubtype subtype)
License requirements: features_modeling ("FEATURES MODELING"), solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.