Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GlobalShapingBuilder.TransitionType |
GlobalShapingBuilder.TransitionType.FUNCTION1
Tangent continuous transition
|
static GlobalShapingBuilder.TransitionType |
GlobalShapingBuilder.TransitionType.FUNCTION2
Position continuous transition
|
static GlobalShapingBuilder.TransitionType |
GlobalShapingBuilder.TransitionType.G2
g2 continuous
|
static GlobalShapingBuilder.TransitionType |
GlobalShapingBuilder.TransitionType.LAW
Transition by law
|
Modifier and Type | Method and Description |
---|---|
GlobalShapingBuilder.TransitionType |
GlobalShapingBuilder.transitionOptions()
Returns the transition options
License requirements: None. |
static GlobalShapingBuilder.TransitionType |
GlobalShapingBuilder.TransitionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GlobalShapingBuilder.TransitionType |
GlobalShapingBuilder.TransitionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GlobalShapingBuilder.TransitionType[] |
GlobalShapingBuilder.TransitionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GlobalShapingBuilder.setTransitionOptions(GlobalShapingBuilder.TransitionType transitionOptions)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.