Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GlobalShapingBuilder.TargetCurveOrientationType |
GlobalShapingBuilder.TargetCurveOrientationType.PARALLEL
Target curve is parallel to the limit curves.
|
static GlobalShapingBuilder.TargetCurveOrientationType |
GlobalShapingBuilder.TargetCurveOrientationType.PERPENDICULAR
Target curves are perpendicular to the limit curves.
|
Modifier and Type | Method and Description |
---|---|
GlobalShapingBuilder.TargetCurveOrientationType |
GlobalShapingBuilder.targetCurveOrientation()
Returns the orientation of the target curve to the limit curves.
|
static GlobalShapingBuilder.TargetCurveOrientationType |
GlobalShapingBuilder.TargetCurveOrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GlobalShapingBuilder.TargetCurveOrientationType |
GlobalShapingBuilder.TargetCurveOrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GlobalShapingBuilder.TargetCurveOrientationType[] |
GlobalShapingBuilder.TargetCurveOrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GlobalShapingBuilder.setTargetCurveOrientation(GlobalShapingBuilder.TargetCurveOrientationType orientation)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.