Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GlobalShapingBuilder.RotationMethodType |
GlobalShapingBuilder.RotationMethodType.ANGLE
Rotation specified by angle
|
static GlobalShapingBuilder.RotationMethodType |
GlobalShapingBuilder.RotationMethodType.DISTANCE
Rotation specified by distance
|
Modifier and Type | Method and Description |
---|---|
GlobalShapingBuilder.RotationMethodType |
GlobalShapingBuilder.rotationType()
Returns the rotation type
License requirements: None. |
static GlobalShapingBuilder.RotationMethodType |
GlobalShapingBuilder.RotationMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GlobalShapingBuilder.RotationMethodType |
GlobalShapingBuilder.RotationMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GlobalShapingBuilder.RotationMethodType[] |
GlobalShapingBuilder.RotationMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GlobalShapingBuilder.setRotationType(GlobalShapingBuilder.RotationMethodType rotationType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.