Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GlobalShapingBuilder.RadiusType |
GlobalShapingBuilder.RadiusType.QUINTIC
Quintic method.
|
static GlobalShapingBuilder.RadiusType |
GlobalShapingBuilder.RadiusType.RADIUS
Radius method.
|
Modifier and Type | Method and Description |
---|---|
GlobalShapingBuilder.RadiusType |
GlobalShapingBuilder.radiusOptions()
Returns the radius options
License requirements: None. |
static GlobalShapingBuilder.RadiusType |
GlobalShapingBuilder.RadiusType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GlobalShapingBuilder.RadiusType |
GlobalShapingBuilder.RadiusType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GlobalShapingBuilder.RadiusType[] |
GlobalShapingBuilder.RadiusType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GlobalShapingBuilder.setRadiusOptions(GlobalShapingBuilder.RadiusType radiusOptions)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.