Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GlobalShapingBuilder.OffsetMethod |
GlobalShapingBuilder.OffsetMethod.CONSTANT
Constant offset
|
static GlobalShapingBuilder.OffsetMethod |
GlobalShapingBuilder.OffsetMethod.CURVE_DEFINED
Curve interpolated
|
static GlobalShapingBuilder.OffsetMethod |
GlobalShapingBuilder.OffsetMethod.LAW_CONTROLLED
Law controlled
|
Modifier and Type | Method and Description |
---|---|
GlobalShapingBuilder.OffsetMethod |
GlobalShapingBuilder.targetCurveOffsetType()
Returns the target curve offset type
License requirements: None. |
static GlobalShapingBuilder.OffsetMethod |
GlobalShapingBuilder.OffsetMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GlobalShapingBuilder.OffsetMethod |
GlobalShapingBuilder.OffsetMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GlobalShapingBuilder.OffsetMethod[] |
GlobalShapingBuilder.OffsetMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GlobalShapingBuilder.setTargetCurveOffsetType(GlobalShapingBuilder.OffsetMethod targetCurveOffsetType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.