Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GlobalShapingBuilder.ModifyMethodType |
GlobalShapingBuilder.ModifyMethodType.OVERCROWN
By Surface overcrown modify
|
static GlobalShapingBuilder.ModifyMethodType |
GlobalShapingBuilder.ModifyMethodType.STRETCH
By Surface stretch modify
|
Modifier and Type | Method and Description |
---|---|
GlobalShapingBuilder.ModifyMethodType |
GlobalShapingBuilder.modifyMethod()
Returns the modify method
License requirements: None. |
static GlobalShapingBuilder.ModifyMethodType |
GlobalShapingBuilder.ModifyMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GlobalShapingBuilder.ModifyMethodType |
GlobalShapingBuilder.ModifyMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GlobalShapingBuilder.ModifyMethodType[] |
GlobalShapingBuilder.ModifyMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GlobalShapingBuilder.setModifyMethod(GlobalShapingBuilder.ModifyMethodType modifyMethod)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.