Package | Description |
---|---|
nxopen.facet |
Provides classes and interfaces for Faceted Representations.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
GeometricConstraintDataManager |
CreateTransitionBuilder.selectedPoints()
Returns the selected points.
|
Modifier and Type | Method and Description |
---|---|
GeometricConstraintDataManager |
StudioSplineBuilderEx.constraintManager()
Returns the constraint manager
License requirements: None. |
GeometricConstraintDataManager |
StudioSplineBuilder.constraintManager()
Deprecated.
Deprecated in NX8.0.0. Use
StudioSplineBuilderEx instead.
|
GeometricConstraintDataManager |
PolylineBuilder.constraintManager()
Returns the constraint manager
License requirements: None. |
GeometricConstraintDataManager |
IsoparametricCurvesBuilder.constraintManager()
Returns the constraint manager.
|
GeometricConstraintDataManager |
FitCurveBuilder.constraintManager()
Returns the constraint manager
License requirements: None. |
GeometricConstraintDataManager |
CurveOnSurfaceBuilder.constraintManager()
Returns the constraint manager
License requirements: solid_modeling ("SOLIDS MODELING") . |
GeometricConstraintDataManager |
GeometricConstraintDataSetManager.createGeometricConstraintDataManager()
Creates a new empty
GeometricConstraintDataManager object
License requirements: None. |
GeometricConstraintDataManager[] |
GeometricConstraintDataSetManager.getContents()
Queries all the manager objects
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Modifier and Type | Method and Description |
---|---|
void |
GeometricConstraintDataSetManager.append(GeometricConstraintDataManager manager)
Appends
GeometricConstraintDataManager object to the end of the list
License requirements: features_modeling ("FEATURES MODELING") Created in NX5.0.0 |
void |
GeometricConstraintDataSetManager.delete(GeometricConstraintDataManager manager)
Deletes
GeometricConstraintDataManager object from the list
License requirements: features_modeling ("FEATURES MODELING") Created in NX5.0.0 |
int |
GeometricConstraintDataSetManager.getIndex(GeometricConstraintDataManager manager)
Finds index of
GeometricConstraintDataManager in the list. |
void |
GeometricConstraintDataSetManager.insert(int insertBeforeIndex,
GeometricConstraintDataManager manager)
Inserts
GeometricConstraintDataManager object in the list
before a given position
License requirements: features_modeling ("FEATURES MODELING") Created in NX5.0.0 |
void |
GeometricConstraintDataSetManager.setContents(GeometricConstraintDataManager[] managers)
Sets array of manager objects in the list.
|
Modifier and Type | Method and Description |
---|---|
GeometricConstraintDataManager |
DeviationGaugeBuilder.constraintManager()
Returns the constraint manager
License requirements: studio_free_form ("STUDIO FREE FORM") . |
GeometricConstraintDataManager |
SurfaceContinuityAnalysisBuilder.dynamicLabel()
Returns the constraint manager
License requirements: None. |
GeometricConstraintDataManager |
DraftAnalysisBuilder.dynamicLabel()
Returns the constraint manager
License requirements: None. |
GeometricConstraintDataManager |
LocalRadiusAnalysisBuilder.selectionPoint()
Returns the selection point
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
GeometricConstraintDataManager |
SelectDividingObjectBuilder.constraintManager()
Returns the iso parameter point
License requirements: None. |
GeometricConstraintDataManager |
CurveShapingBuilder.constraintManager()
Returns the constraint manager.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.