Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Method and Description |
---|---|
GeometricConstraintData |
GeometricConstraintDataManager.createGeometricConstraintData()
Creates a new empty
GeometricConstraintData object
License requirements: None. |
GeometricConstraintData |
GeometricConstraintDataManager.findItem(int constraintIndex)
Returns
GeometricConstraintData object at the input index. |
GeometricConstraintData[] |
GeometricConstraintDataManager.getContents()
Queries all the
GeometricConstraintData objects
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
GeometricConstraintDataManager.append(GeometricConstraintData constraint)
Appends
GeometricConstraintData object to the end of the list
License requirements: None. |
void |
GeometricConstraintDataManager.delete(GeometricConstraintData constraint)
Deletes a given
GeometricConstraintData object from the list
License requirements: None. |
int |
GeometricConstraintDataManager.getIndex(GeometricConstraintData constraint)
Finds index of
GeometricConstraintData object in the list
License requirements: None. |
void |
GeometricConstraintDataManager.insert(int insertBeforeIndex,
GeometricConstraintData constraint)
Inserts
GeometricConstraintData object in the list
before a given position
License requirements: None. |
void |
GeometricConstraintDataManager.setContents(GeometricConstraintData[] constraints)
Sets array of
GeometricConstraintData objects in the list. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.