Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GeomcopyBuilder.AlongPathDistanceOptions |
GeomcopyBuilder.AlongPathDistanceOptions.ARC_LENGTH
arc length option
|
static GeomcopyBuilder.AlongPathDistanceOptions |
GeomcopyBuilder.AlongPathDistanceOptions.FILL_PATH_LENGTH
fill path length option
|
Modifier and Type | Method and Description |
---|---|
GeomcopyBuilder.AlongPathDistanceOptions |
GeomcopyBuilder.fillPathLength()
Returns the fill path length, a distance option for along path type of instancing.
|
static GeomcopyBuilder.AlongPathDistanceOptions |
GeomcopyBuilder.AlongPathDistanceOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeomcopyBuilder.AlongPathDistanceOptions |
GeomcopyBuilder.AlongPathDistanceOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeomcopyBuilder.AlongPathDistanceOptions[] |
GeomcopyBuilder.AlongPathDistanceOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeomcopyBuilder.setFillPathLength(GeomcopyBuilder.AlongPathDistanceOptions fillPathLength)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.