Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GeodesicIntersectBuilder.Type |
GeodesicIntersectBuilder.Type.CURVE
Curve.
|
static GeodesicIntersectBuilder.Type |
GeodesicIntersectBuilder.Type.DATUM
Datum.
|
static GeodesicIntersectBuilder.Type |
GeodesicIntersectBuilder.Type.FACE
Face.
|
Modifier and Type | Method and Description |
---|---|
GeodesicIntersectBuilder.Type |
GeodesicIntersectBuilder.intersectType()
Returns the intersect type
License requirements: None. |
static GeodesicIntersectBuilder.Type |
GeodesicIntersectBuilder.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeodesicIntersectBuilder.Type |
GeodesicIntersectBuilder.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeodesicIntersectBuilder.Type[] |
GeodesicIntersectBuilder.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeodesicIntersectBuilder.setIntersectType(GeodesicIntersectBuilder.Type intersectType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.