Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FlatteningAndFormingBuilder.Types |
FlatteningAndFormingBuilder.Types.CALCULATION
This option faces to be flattened will be used to calculate the mapping.
|
static FlatteningAndFormingBuilder.Types |
FlatteningAndFormingBuilder.Types.REUSE
This option uses a transformation maping of an existing flattening feature to reapply it in its original or reversed direction to additional transformation objects.
|
Modifier and Type | Method and Description |
---|---|
FlatteningAndFormingBuilder.Types |
FlatteningAndFormingBuilder.type()
Returns the type
License requirements: None. |
static FlatteningAndFormingBuilder.Types |
FlatteningAndFormingBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlatteningAndFormingBuilder.Types |
FlatteningAndFormingBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlatteningAndFormingBuilder.Types[] |
FlatteningAndFormingBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlatteningAndFormingBuilder.setType(FlatteningAndFormingBuilder.Types type)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.