Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FlatteningAndFormingBuilder.DistortionMap |
FlatteningAndFormingBuilder.DistortionMap.ANGLE
Shear distortion of U/V directions
|
static FlatteningAndFormingBuilder.DistortionMap |
FlatteningAndFormingBuilder.DistortionMap.AREA
Distortion of area
|
static FlatteningAndFormingBuilder.DistortionMap |
FlatteningAndFormingBuilder.DistortionMap.LENGTH
Distortion of length
|
static FlatteningAndFormingBuilder.DistortionMap |
FlatteningAndFormingBuilder.DistortionMap.NONE
No distortion map
|
Modifier and Type | Method and Description |
---|---|
FlatteningAndFormingBuilder.DistortionMap |
FlatteningAndFormingBuilder.distortionMapOptions()
Returns the option to display the distortion map on the source faces.
|
static FlatteningAndFormingBuilder.DistortionMap |
FlatteningAndFormingBuilder.DistortionMap.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlatteningAndFormingBuilder.DistortionMap |
FlatteningAndFormingBuilder.DistortionMap.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlatteningAndFormingBuilder.DistortionMap[] |
FlatteningAndFormingBuilder.DistortionMap.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlatteningAndFormingBuilder.setDistortionMapOptions(FlatteningAndFormingBuilder.DistortionMap distortionMapOptions)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.