Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FitSurfaceBuilder.DirectionType |
FitSurfaceBuilder.DirectionType.BEST_FIT
The fit target is sort of rectangular.
|
static FitSurfaceBuilder.DirectionType |
FitSurfaceBuilder.DirectionType.CSYS
CSYS will specify same as orientation but with the need to make it associative with existing geometry.
|
static FitSurfaceBuilder.DirectionType |
FitSurfaceBuilder.DirectionType.ORIENTATION
Orientation will specify the direction and U/V orientation.
|
static FitSurfaceBuilder.DirectionType |
FitSurfaceBuilder.DirectionType.VECTOR
Vector will specify the fit direction.
|
Modifier and Type | Method and Description |
---|---|
FitSurfaceBuilder.DirectionType |
FitSurfaceBuilder.directionOption()
Returns the direction option
License requirements: None. |
static FitSurfaceBuilder.DirectionType |
FitSurfaceBuilder.DirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FitSurfaceBuilder.DirectionType |
FitSurfaceBuilder.DirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FitSurfaceBuilder.DirectionType[] |
FitSurfaceBuilder.DirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FitSurfaceBuilder.setDirectionOption(FitSurfaceBuilder.DirectionType directionOption)
License requirements: nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.