Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FeatureCollection.ReorderType |
FeatureCollection.ReorderType.AFTER |
static FeatureCollection.ReorderType |
FeatureCollection.ReorderType.BEFORE |
static FeatureCollection.ReorderType |
FeatureCollection.ReorderType.INTO |
Modifier and Type | Method and Description |
---|---|
static FeatureCollection.ReorderType |
FeatureCollection.ReorderType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FeatureCollection.ReorderType |
FeatureCollection.ReorderType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FeatureCollection.ReorderType[] |
FeatureCollection.ReorderType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FeatureCollection.reorderFeature(Feature[] features,
Feature target,
FeatureCollection.ReorderType beforeOrAfter)
Reorders the Feature with respect to the given feature
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
FeatureCollection.reorganizeFeature(Feature[] features,
Feature target,
FeatureCollection.ReorderType beforeOrAfter)
Reorganizes the Feature with respect to the given feature across the part module
License requirements: usr_defined_features ("USER DEFINED FEATURES") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.