Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static Feature.DiagnosticType |
Feature.DiagnosticType.INFORMATION
Information alert
|
static Feature.DiagnosticType |
Feature.DiagnosticType.WARNING
Warning
|
Modifier and Type | Method and Description |
---|---|
static Feature.DiagnosticType |
Feature.DiagnosticType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Feature.DiagnosticType |
Feature.DiagnosticType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Feature.DiagnosticType[] |
Feature.DiagnosticType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Feature.logDiagnostic(int errorCode,
String message,
Feature.DiagnosticType diagnosticType)
Log a diagnostic alert for this feature
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.