Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static Feature.BooleanType |
Feature.BooleanType.CREATE
Create
|
static Feature.BooleanType |
Feature.BooleanType.EMBOSS_NORMAL_SIDE
Emboss, keep tool on normal side of sheet
|
static Feature.BooleanType |
Feature.BooleanType.EMBOSS_OPPOSITE_NORMAL_SIDE
Emboss, keep tool opposite of normal side of sheet
|
static Feature.BooleanType |
Feature.BooleanType.INTERSECT
Intersect
|
static Feature.BooleanType |
Feature.BooleanType.SUBTRACT
Subtract
|
static Feature.BooleanType |
Feature.BooleanType.UNITE
Unite
|
Modifier and Type | Method and Description |
---|---|
Feature.BooleanType |
BlockFeatureBuilder.booleanType()
Returns the boolean operation for the block
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Feature.BooleanType |
BooleanBuilder.operation()
Returns the boolean operation
License requirements: None. |
static Feature.BooleanType |
Feature.BooleanType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Feature.BooleanType |
Feature.BooleanType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Feature.BooleanType[] |
Feature.BooleanType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BlockFeatureBuilder.setBooleanOperationAndTarget(Feature.BooleanType booleanOperation,
Body targetBody)
Set the boolean operation for creating the block and the boolean operation target body
License requirements: solid_modeling ("SOLIDS MODELING") OR features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
BlockFeatureBuilder.setBooleanType(Feature.BooleanType booleanType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
BooleanBuilder.setOperation(Feature.BooleanType operation)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.