Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FaceBlendBuilder.WidthMethod |
FaceBlendBuilder.WidthMethod.FORCED_CONSTANT
Forced Constant
|
static FaceBlendBuilder.WidthMethod |
FaceBlendBuilder.WidthMethod.NATURALLY_VARYING
Naturally Varying
|
static FaceBlendBuilder.WidthMethod |
FaceBlendBuilder.WidthMethod.TWO_CONSTRAINT_CURVES
Two Constraint Curves
|
Modifier and Type | Method and Description |
---|---|
FaceBlendBuilder.WidthMethod |
FaceBlendBuilder.blendWidthMethod()
Returns the width method for face blend
License requirements: solid_modeling ("SOLIDS MODELING") . |
static FaceBlendBuilder.WidthMethod |
FaceBlendBuilder.WidthMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FaceBlendBuilder.WidthMethod |
FaceBlendBuilder.WidthMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FaceBlendBuilder.WidthMethod[] |
FaceBlendBuilder.WidthMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FaceBlendBuilder.setBlendWidthMethod(FaceBlendBuilder.WidthMethod method)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.