Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FaceBlendBuilder.Type |
FaceBlendBuilder.Type.ROLLING_BALL |
static FaceBlendBuilder.Type |
FaceBlendBuilder.Type.SWEPT |
Modifier and Type | Method and Description |
---|---|
FaceBlendBuilder.Type |
FaceBlendBuilder.blendType()
Returns the type for face blend
License requirements: None. |
static FaceBlendBuilder.Type |
FaceBlendBuilder.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FaceBlendBuilder.Type |
FaceBlendBuilder.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FaceBlendBuilder.Type[] |
FaceBlendBuilder.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FaceBlendBuilder.setBlendType(FaceBlendBuilder.Type type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.