Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FaceBlendBuilder.TrimmingMethod |
FaceBlendBuilder.TrimmingMethod.LONG
Trim long
|
static FaceBlendBuilder.TrimmingMethod |
FaceBlendBuilder.TrimmingMethod.NONE
No trim
|
static FaceBlendBuilder.TrimmingMethod |
FaceBlendBuilder.TrimmingMethod.SHORT
Trim short
|
static FaceBlendBuilder.TrimmingMethod |
FaceBlendBuilder.TrimmingMethod.TO_ALL_FACES
Trim to all faces
|
Modifier and Type | Method and Description |
---|---|
FaceBlendBuilder.TrimmingMethod |
FaceBlendBuilder.trimmingOption()
Returns the trimming option for face blend
License requirements: None. |
static FaceBlendBuilder.TrimmingMethod |
FaceBlendBuilder.TrimmingMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FaceBlendBuilder.TrimmingMethod |
FaceBlendBuilder.TrimmingMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FaceBlendBuilder.TrimmingMethod[] |
FaceBlendBuilder.TrimmingMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FaceBlendBuilder.setTrimmingOption(FaceBlendBuilder.TrimmingMethod trimmingOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.