Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FaceBlendBuilder.DefiningType |
FaceBlendBuilder.DefiningType.BLEND_FROM_EDGES |
static FaceBlendBuilder.DefiningType |
FaceBlendBuilder.DefiningType.BLEND_THREE_FACE
this is form new three face blend
|
static FaceBlendBuilder.DefiningType |
FaceBlendBuilder.DefiningType.BLEND_TWO_FACE
this is for normal two face blend
|
Modifier and Type | Method and Description |
---|---|
FaceBlendBuilder.DefiningType |
FaceBlendBuilder.faceBlendDefineType()
Returns the face blend defining type get
License requirements: None. |
static FaceBlendBuilder.DefiningType |
FaceBlendBuilder.DefiningType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FaceBlendBuilder.DefiningType |
FaceBlendBuilder.DefiningType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FaceBlendBuilder.DefiningType[] |
FaceBlendBuilder.DefiningType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FaceBlendBuilder.setFaceBlendDefineType(FaceBlendBuilder.DefiningType type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.