Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ExtensionBuilder.Types |
ExtensionBuilder.Types.CORNER |
static ExtensionBuilder.Types |
ExtensionBuilder.Types.EDGE |
Modifier and Type | Method and Description |
---|---|
ExtensionBuilder.Types |
ExtensionBuilder.type()
Returns the type
License requirements: None. |
static ExtensionBuilder.Types |
ExtensionBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtensionBuilder.Types |
ExtensionBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtensionBuilder.Types[] |
ExtensionBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExtensionBuilder.setType(ExtensionBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") OR free_form_modeling ("FREE-FORM MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.