Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ExtendSheetBuilder.SideEdgeShape |
ExtendSheetBuilder.SideEdgeShape.AUTOMATIC |
static ExtendSheetBuilder.SideEdgeShape |
ExtendSheetBuilder.SideEdgeShape.ORTHOGONAL |
static ExtendSheetBuilder.SideEdgeShape |
ExtendSheetBuilder.SideEdgeShape.TANGENT |
Modifier and Type | Method and Description |
---|---|
ExtendSheetBuilder.SideEdgeShape |
ExtendSheetBuilder.sideEdgeShapeOption()
Returns the direction by which the edge is extended
License requirements: None. |
static ExtendSheetBuilder.SideEdgeShape |
ExtendSheetBuilder.SideEdgeShape.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtendSheetBuilder.SideEdgeShape |
ExtendSheetBuilder.SideEdgeShape.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtendSheetBuilder.SideEdgeShape[] |
ExtendSheetBuilder.SideEdgeShape.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExtendSheetBuilder.setSideEdgeShapeOption(ExtendSheetBuilder.SideEdgeShape sideEdgeShapeOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.