Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ExtendSheetBuilder.Limit |
ExtendSheetBuilder.Limit.OFFSET
Limit by offset distance
|
static ExtendSheetBuilder.Limit |
ExtendSheetBuilder.Limit.UNTIL_SELECTED
Limit by selected face/plane
|
Modifier and Type | Method and Description |
---|---|
ExtendSheetBuilder.Limit |
ExtendSheetBuilder.limitMethod()
Returns the option to control limit by distance or until selected objects
License requirements: None. |
static ExtendSheetBuilder.Limit |
ExtendSheetBuilder.Limit.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtendSheetBuilder.Limit |
ExtendSheetBuilder.Limit.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtendSheetBuilder.Limit[] |
ExtendSheetBuilder.Limit.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExtendSheetBuilder.setLimitMethod(ExtendSheetBuilder.Limit limitMethod)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.