Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ExtendSheetBuilder.BodyOutput |
ExtendSheetBuilder.BodyOutput.EXTEND_ORIGINAL_SHEET |
static ExtendSheetBuilder.BodyOutput |
ExtendSheetBuilder.BodyOutput.EXTENDAS_NEW_FACE |
static ExtendSheetBuilder.BodyOutput |
ExtendSheetBuilder.BodyOutput.EXTENDAS_NEW_SHEET |
Modifier and Type | Method and Description |
---|---|
ExtendSheetBuilder.BodyOutput |
TrimAndExtendBuilder.bodyOutputOption()
Returns the body output type
License requirements: None. |
ExtendSheetBuilder.BodyOutput |
ExtendSheetBuilder.bodyOutputOption()
Returns the option to control whether the shape is extended as the original sheet, as a new face, or as a new sheet
License requirements: None. |
static ExtendSheetBuilder.BodyOutput |
ExtendSheetBuilder.BodyOutput.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtendSheetBuilder.BodyOutput |
ExtendSheetBuilder.BodyOutput.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtendSheetBuilder.BodyOutput[] |
ExtendSheetBuilder.BodyOutput.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimAndExtendBuilder.setBodyOutputOption(ExtendSheetBuilder.BodyOutput bodyOutputOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
ExtendSheetBuilder.setBodyOutputOption(ExtendSheetBuilder.BodyOutput bodyOutputOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.