Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EmbossSidewall.SidewallMethod |
EmbossSidewall.SidewallMethod.CURVE_TAPERED
Indicates method to calculate tapered sidewall faces with reference to the taper direction.
|
static EmbossSidewall.SidewallMethod |
EmbossSidewall.SidewallMethod.ISOCLINE_TAPERED
Indicates method to calculate tapered sidewall faces with reference to the taper direction and the taper reference curve tangents.
|
static EmbossSidewall.SidewallMethod |
EmbossSidewall.SidewallMethod.NORMAL
Indicates method to calculate tapered sidewall faces with reference to the taper direction and the normal of the taper faces' original surfaces.
|
static EmbossSidewall.SidewallMethod |
EmbossSidewall.SidewallMethod.OFFSET
(Not supported in NX4.)
|
static EmbossSidewall.SidewallMethod |
EmbossSidewall.SidewallMethod.RULED
Indicates method to create sidewalls that are ruled along the normals of the faces in the supplied profile.
|
static EmbossSidewall.SidewallMethod |
EmbossSidewall.SidewallMethod.SWEPT
Indicates method to create sidewalls that are swept.
|
static EmbossSidewall.SidewallMethod |
EmbossSidewall.SidewallMethod.TWO_SECTION
(Not supported in NX4.)
|
Modifier and Type | Method and Description |
---|---|
EmbossSidewall.SidewallMethod |
EmbossSidewall.sidewallOption()
Returns the method to create sidewall
License requirements: None. |
static EmbossSidewall.SidewallMethod |
EmbossSidewall.SidewallMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbossSidewall.SidewallMethod |
EmbossSidewall.SidewallMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbossSidewall.SidewallMethod[] |
EmbossSidewall.SidewallMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EmbossSidewall.setSidewallOption(EmbossSidewall.SidewallMethod sidewallMethod)
Sets the method to create sidewall
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.