Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EmbossRegion.ConvexityOption |
EmbossRegion.ConvexityOption.ABOVE
Indicates the emboss geometry is above the target("Pad").
|
static EmbossRegion.ConvexityOption |
EmbossRegion.ConvexityOption.BELOW
Indicates the emboss geometry is below the target("Pocket").
|
static EmbossRegion.ConvexityOption |
EmbossRegion.ConvexityOption.MIXED
Indicates the emboss geometry is both above and below the Target("Mixed").
|
Modifier and Type | Method and Description |
---|---|
EmbossRegion.ConvexityOption |
EmbossRegion.convexity()
Returns the convexity option
License requirements: None. |
static EmbossRegion.ConvexityOption |
EmbossRegion.ConvexityOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbossRegion.ConvexityOption |
EmbossRegion.ConvexityOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbossRegion.ConvexityOption[] |
EmbossRegion.ConvexityOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EmbossRegion.setConvexity(EmbossRegion.ConvexityOption convexity)
Sets the convexity option
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.