Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EmbossProjection.ProjectionOption |
EmbossProjection.ProjectionOption.ENDCAP
Indicates the geometry is End-Cap.
|
static EmbossProjection.ProjectionOption |
EmbossProjection.ProjectionOption.FACE
Indicates the geometries are selected faces.
|
static EmbossProjection.ProjectionOption |
EmbossProjection.ProjectionOption.NONE
Indicates no geometry.
|
static EmbossProjection.ProjectionOption |
EmbossProjection.ProjectionOption.PLANE
Indicates the geometry is datum plane.
|
static EmbossProjection.ProjectionOption |
EmbossProjection.ProjectionOption.TARGET
Indicates the geometry is target.
|
Modifier and Type | Method and Description |
---|---|
EmbossProjection.ProjectionOption |
EmbossProjection.option()
Returns the projection option
License requirements: solid_modeling ("SOLIDS MODELING") . |
static EmbossProjection.ProjectionOption |
EmbossProjection.ProjectionOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbossProjection.ProjectionOption |
EmbossProjection.ProjectionOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbossProjection.ProjectionOption[] |
EmbossProjection.ProjectionOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EmbossProjection.setOption(EmbossProjection.ProjectionOption option)
Sets the projection option
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.