Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EmbedManagerBuilder.UsageAreaTypes |
EmbedManagerBuilder.UsageAreaTypes.MATH_WORKSHEET
Used by Symbolica and Maple applications.
|
Modifier and Type | Method and Description |
---|---|
EmbedManagerBuilder.UsageAreaTypes |
EmbedManagerBuilder.area()
Returns the area in the parts file which matches the application usage.
|
static EmbedManagerBuilder.UsageAreaTypes |
EmbedManagerBuilder.UsageAreaTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbedManagerBuilder.UsageAreaTypes |
EmbedManagerBuilder.UsageAreaTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbedManagerBuilder.UsageAreaTypes[] |
EmbedManagerBuilder.UsageAreaTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EmbedManagerBuilder.setArea(EmbedManagerBuilder.UsageAreaTypes area)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.