Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EmbedManagerBuilder.TaskTypes |
EmbedManagerBuilder.TaskTypes.DELETE
Delete the existing embedded file.
|
static EmbedManagerBuilder.TaskTypes |
EmbedManagerBuilder.TaskTypes.EMBED
Embed operating system file in part.
|
static EmbedManagerBuilder.TaskTypes |
EmbedManagerBuilder.TaskTypes.RENAME
Rename the existing embedded file.
|
static EmbedManagerBuilder.TaskTypes |
EmbedManagerBuilder.TaskTypes.REPLACE
Replace the existing embedded file.
|
Modifier and Type | Method and Description |
---|---|
EmbedManagerBuilder.TaskTypes |
EmbedManagerBuilder.task()
Returns the task to be performed.
|
static EmbedManagerBuilder.TaskTypes |
EmbedManagerBuilder.TaskTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbedManagerBuilder.TaskTypes |
EmbedManagerBuilder.TaskTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbedManagerBuilder.TaskTypes[] |
EmbedManagerBuilder.TaskTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EmbedManagerBuilder.setTask(EmbedManagerBuilder.TaskTypes type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.