Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EmbedManagerBuilder.LocationTypes |
EmbedManagerBuilder.LocationTypes.OPERATING_SYSTEM
File exists on the native OS.
|
static EmbedManagerBuilder.LocationTypes |
EmbedManagerBuilder.LocationTypes.TEAMCENTER
File exists in Teamcenter.
|
Modifier and Type | Method and Description |
---|---|
EmbedManagerBuilder.LocationTypes |
EmbedManagerBuilder.location()
Returns the source location of the file.
|
static EmbedManagerBuilder.LocationTypes |
EmbedManagerBuilder.LocationTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbedManagerBuilder.LocationTypes |
EmbedManagerBuilder.LocationTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbedManagerBuilder.LocationTypes[] |
EmbedManagerBuilder.LocationTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EmbedManagerBuilder.setLocation(EmbedManagerBuilder.LocationTypes location)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.