Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EdgeSymmetryBuilder.MovementMethods |
EdgeSymmetryBuilder.MovementMethods.NORMAL
Does a normal match
|
static EdgeSymmetryBuilder.MovementMethods |
EdgeSymmetryBuilder.MovementMethods.PROJECT
Does a match by projecting poles corresponding to target edge of the surface
|
static EdgeSymmetryBuilder.MovementMethods |
EdgeSymmetryBuilder.MovementMethods.WCS
Does a match by moving poles along a WCS principal axis direction
|
Modifier and Type | Method and Description |
---|---|
EdgeSymmetryBuilder.MovementMethods |
EdgeSymmetryBuilder.movementMethod()
Returns the pole movement method to be used in matching process
License requirements: None. |
static EdgeSymmetryBuilder.MovementMethods |
EdgeSymmetryBuilder.MovementMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeSymmetryBuilder.MovementMethods |
EdgeSymmetryBuilder.MovementMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeSymmetryBuilder.MovementMethods[] |
EdgeSymmetryBuilder.MovementMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeSymmetryBuilder.setMovementMethod(EdgeSymmetryBuilder.MovementMethods movementMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.