Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EdgeBlendBuilder.Section |
EdgeBlendBuilder.Section.CIRCULAR
Default option, circular shaped blends
|
static EdgeBlendBuilder.Section |
EdgeBlendBuilder.Section.CONIC
Conical shaped blends
|
EdgeBlendBuilder.Section |
EdgeBlendBuilder.ChainsetAndSectionValueData.sectiontype
The section type of this chain set collector
|
Modifier and Type | Method and Description |
---|---|
static EdgeBlendBuilder.Section |
EdgeBlendBuilder.Section.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeBlendBuilder.Section |
EdgeBlendBuilder.Section.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeBlendBuilder.Section[] |
EdgeBlendBuilder.Section.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
int |
EdgeBlendBuilder.addChainset(ScCollector collector,
EdgeBlendBuilder.Section sectionType,
EdgeBlendBuilder.Conic conicMethod,
EdgeBlendBuilder.Rhotype rhoType,
String radius,
String center,
String rho)
Add an edge blend chainset to the edge blend
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.