Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EdgeBlendBuilder.Overlap |
EdgeBlendBuilder.Overlap.ANY_CONVEXITY_ROLL_OVER
Any convexity,roll over
|
static EdgeBlendBuilder.Overlap |
EdgeBlendBuilder.Overlap.DIFFERENT_CONVEXITY_ROLL_OVER
If different convexity,roll over
|
static EdgeBlendBuilder.Overlap |
EdgeBlendBuilder.Overlap.MAINTAIN_AND_INTERSECT
Maintain Blend and Intersect
|
Modifier and Type | Method and Description |
---|---|
EdgeBlendBuilder.Overlap |
EdgeBlendBuilder.overlapOption()
Returns the overlap resolution for edge blend
License requirements: None. |
static EdgeBlendBuilder.Overlap |
EdgeBlendBuilder.Overlap.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeBlendBuilder.Overlap |
EdgeBlendBuilder.Overlap.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeBlendBuilder.Overlap[] |
EdgeBlendBuilder.Overlap.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeBlendBuilder.setOverlapOption(EdgeBlendBuilder.Overlap overlapOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.