Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EdgeBlendBuilder.FaceContinuity |
EdgeBlendBuilder.FaceContinuity.CURVATURE |
static EdgeBlendBuilder.FaceContinuity |
EdgeBlendBuilder.FaceContinuity.TANGENT |
Modifier and Type | Method and Description |
---|---|
EdgeBlendBuilder.FaceContinuity |
EdgeBlendBuilder.blendFaceContinuity()
Returns the Blend Face Continuity option
License requirements: None. |
static EdgeBlendBuilder.FaceContinuity |
EdgeBlendBuilder.FaceContinuity.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgeBlendBuilder.FaceContinuity |
EdgeBlendBuilder.FaceContinuity.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgeBlendBuilder.FaceContinuity[] |
EdgeBlendBuilder.FaceContinuity.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgeBlendBuilder.setBlendFaceContinuity(EdgeBlendBuilder.FaceContinuity optionValue)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.