Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DraftBuilder.Type |
DraftBuilder.Type.EDGE
From Edges type
|
static DraftBuilder.Type |
DraftBuilder.Type.FACE
Face Draft type
|
static DraftBuilder.Type |
DraftBuilder.Type.PARTING_EDGE
Draft with Parting Edges type
|
static DraftBuilder.Type |
DraftBuilder.Type.TANGENT
Tangent Draft type
|
Modifier and Type | Method and Description |
---|---|
DraftBuilder.Type |
DraftBuilder.typeOfDraft()
Returns the Draft type
License requirements: solid_modeling ("SOLIDS MODELING") . |
static DraftBuilder.Type |
DraftBuilder.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DraftBuilder.Type |
DraftBuilder.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DraftBuilder.Type[] |
DraftBuilder.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DraftBuilder.setTypeOfDraft(DraftBuilder.Type type)
Sets the Draft type
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.