Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DraftBuilder.DraftReferencesMethods |
DraftBuilder.DraftReferencesMethods.PARTING_FACE
Draft from stationary parting face.
|
static DraftBuilder.DraftReferencesMethods |
DraftBuilder.DraftReferencesMethods.STATIONARY_AND_PARTING_FACE
Draft from stationary face to parting face.
|
static DraftBuilder.DraftReferencesMethods |
DraftBuilder.DraftReferencesMethods.STATIONARY_FACE
Draft from stationary face.
|
Modifier and Type | Method and Description |
---|---|
DraftBuilder.DraftReferencesMethods |
DraftBuilder.draftReferencesMethod()
Returns the draft references method
License requirements: None. |
static DraftBuilder.DraftReferencesMethods |
DraftBuilder.DraftReferencesMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DraftBuilder.DraftReferencesMethods |
DraftBuilder.DraftReferencesMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DraftBuilder.DraftReferencesMethods[] |
DraftBuilder.DraftReferencesMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DraftBuilder.setDraftReferencesMethod(DraftBuilder.DraftReferencesMethods draftReferencesMethod)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.