Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DraftBodyBuilder.Types |
DraftBodyBuilder.Types.EDGES
From Edges
|
static DraftBodyBuilder.Types |
DraftBodyBuilder.Types.FACES
Faces to Draft
|
Modifier and Type | Method and Description |
---|---|
DraftBodyBuilder.Types |
DraftBodyBuilder.type()
Returns the draft body type
License requirements: None. |
static DraftBodyBuilder.Types |
DraftBodyBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DraftBodyBuilder.Types |
DraftBodyBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DraftBodyBuilder.Types[] |
DraftBodyBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DraftBodyBuilder.setType(DraftBodyBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.