Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DraftBodyBuilder.RepairOption |
DraftBodyBuilder.RepairOption.BLENDS
Repair concave miter corners with blends
|
static DraftBodyBuilder.RepairOption |
DraftBodyBuilder.RepairOption.BOTH
Repair concave miter corners with both blends and planes
|
static DraftBodyBuilder.RepairOption |
DraftBodyBuilder.RepairOption.NONE
No repair option is specified
|
static DraftBodyBuilder.RepairOption |
DraftBodyBuilder.RepairOption.PLANES
Repair concave miter corners with planes
|
Modifier and Type | Method and Description |
---|---|
DraftBodyBuilder.RepairOption |
DraftBodyBuilder.repairingOption()
Deprecated.
Deprecated in NX9.0.0. Use
DraftBodyBuilder.repairPartingEdge() instead
|
static DraftBodyBuilder.RepairOption |
DraftBodyBuilder.RepairOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DraftBodyBuilder.RepairOption |
DraftBodyBuilder.RepairOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DraftBodyBuilder.RepairOption[] |
DraftBodyBuilder.RepairOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DraftBodyBuilder.setRepairingOption(DraftBodyBuilder.RepairOption repairingOption)
Deprecated.
Deprecated in NX9.0.0. Use
DraftBodyBuilder.setRepairPartingEdge(nxopen.features.DraftBodyBuilder.RepairingPartingEdgeOption) instead
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.