Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DraftBodyBuilder.Method |
DraftBodyBuilder.Method.ISOCLINE
Indicates use of isocline algorithm to create draft.
|
static DraftBodyBuilder.Method |
DraftBodyBuilder.Method.TRUE_DRAFT
Indicates use of true draft algorithm to create draft.
|
Modifier and Type | Method and Description |
---|---|
DraftBodyBuilder.Method |
DraftBodyBuilder.draftMethod()
Returns the draft method
License requirements: None. |
static DraftBodyBuilder.Method |
DraftBodyBuilder.Method.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DraftBodyBuilder.Method |
DraftBodyBuilder.Method.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DraftBodyBuilder.Method[] |
DraftBodyBuilder.Method.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DraftBodyBuilder.setDraftMethod(DraftBodyBuilder.Method draftMethod)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.